Technical FAQs

Ask a Question

What is the difference in Heavy Duty switch Horsepower ratings ``Standard`` and ``Max``?

``Standard`` HP rating applies when using fast acting fuses. ``Max`` HP rating applies when using dual element time-delay fuses in the switch.


CTA-ID : 114
Was this helpful?
What can we do to improve the information ?