Technical FAQs

Ask a Question

G30T33 - Are these thermal units for the old Telemecanique / Gould ITE Starters still available?

No, parts are currently obsolete and no longer available.Suggest customer replace complete starter with Class 8536, select type based on application.


CTA-ID : 565
Was this helpful?
What can we do to improve the information ?