Technical FAQs

Ask a Question

What does the form on 9007CR61B2Y225 mean?

Form Y225 changes the conduit entry to 3/4``. This form is a factory option, not field installable. Because the 9007CR requires factory mating of both pieces of the enclosure, purchase of the mounting receptacle only is not possible. If the device were a standard 9007C plug in unit, the housing could be replaced using, for example, 9007CT54Y225


CTA-ID : 1130
Was this helpful?
What can we do to improve the information ?