Technical FAQs

Ask a Question

Are Class 8903 Electrically Held Lighting Contactors available in single pole versions?

No, Class 8903 Type L are available in 2 through 12 pole versions and Class 8903 Type S are available in 2 through 5 pole versions for 30/60/100/200 amp, and 2 & 3 pole versions on 300/400/600/800 amp devices.


CTA-ID : 847
Was this helpful?
What can we do to improve the information ?