Technical FAQs

Ask a Question

Is the 125 A 3-pole breaker on a NQOD panel a bolt on breaker?

All QO and QOB 3-pole breakers above 100 A are bolt on .


CTA-ID : 417
Was this helpful?
What can we do to improve the information ?