Technical FAQs

Ask a Question

What is the largest branch breaker that can be installed in an NQOD442L225 Interior?

Issue:
Product Selection

Product Line:
Panelboards

Environment:

UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17

Cause:
Determining the highest ampacity branch device can be important in determining if a panelboard is suitable for serving a load.

Resolution:

The largest breaker that can be branch mounted in an NQOD442L225 interior is the QOB3150VH breaker. The breaker requires 6 pole spaces and the maximum amperage breaker that can be mounted across from it is 20A.  NOTE:  NQOD panelboards are obsolete, superseded by NQ.




 
Was this helpful?
What can we do to improve the information ?