Technical FAQs

Ask a Question

Are Class 8903 Mechanically Held Lighting Contactors available in single pole versions?

No, Class 8903 Type LX are available in 2 through 12 pole versions and Class 8903 Type S are available in 2 through 5 pole versions for 30/60/100 amp, 2 through 4 pole versions on 200 amp, and 2 & 3 pole versions on 300/400/600/800 amp devices.


CTA-ID : 838
Was this helpful?
What can we do to improve the information ?