Technical FAQs

Ask a Question

QO140M200 - What is the temperature rating of the main lugs?<br />

The lugs on the QOM2200VH main breaker are rated for 75 degree C conductors.


CTA-ID : 811
Was this helpful?
What can we do to improve the information ?