Technical FAQs

Ask a Question

Does the white pigtail need to be connected to the panel neutral if there is no load neutral conductor?

Yes, the pigtail connection is needed to power the tripping solenoid and the PTT button.

CTA-ID : 448
Was this helpful?
What can we do to improve the information ?