Technical FAQs

Ask a Question

Can sub-feed lugs be field installed on a 400A NQOD panel?

Issue:
Product Features

Product Line:
Panelboards

Environment:

UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17

Cause:
It may be desirable to add sub-feed lugs after a panelboard has been ordered, shipped, received, or installed.

Resolution:

No. Sub-feed lugs on 400A NQOD panels are available as a factory assembled option ONLY.
NOTE:  NQOD panelboards are obsolete, superseded by NQ.
Was this helpful?
What can we do to improve the information ?