Technical FAQs

Ask a Question

Does the NQOD 100 A main lug only 30-circuit panel with subfeed lugs require a larger enclosure?

Issue:
Product Features

Product Line:
Panelboards

Environment:

UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17

Cause:
Concern over product dimensions:  Sub-feed lugs often necessitate a larger enclosure to accommodate additional wire bending space.

Resolution:

No.  NOTE:  NQOD panelboards are obsolete, superseded by NQ.


 
Was this helpful?
What can we do to improve the information ?