Technical FAQs

Ask a Question

Is an NQOD panelboard available in a single enclosure with a factory installed XGA or IMA TVSS with 400 A main circuit breaker and subfeed circuit breakers?

Issue:
Product Features

Product Line:
Panelboards

Environment:

UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17


Cause:
It can be desirable to locate a surge protective device within a panelboard enclosure for economy of wall space as well as optimum surge protection.

Resolution:

No. The TVSS unit must be remote mounted (external).  NOTE: NQOD panelboards are obsolete, superseded by NQ.


 
Was this helpful?
What can we do to improve the information ?