Technical FAQs

Ask a Question

What is the minimum load rating for the low level aux. contact on NSE breakers vs. standard level?

The low level aux. contacts have a minimum load rating of 1mA at 4V and the standard level aux. contacts have a minimum rating of 10mA at 24V.




CTA-ID : 818
Was this helpful?
What can we do to improve the information ?