Technical FAQs

Ask a Question

Does the HU365AWK have knockouts.

No knockouts are provided on NEMA Type 12 switches with AWK suffix. If knockouts are required, consider NEMA Type 12K switches with A suffix. However, NEMA Type 12K switches are available only through 200 ampere.

CTA-ID : 781
Was this helpful?
What can we do to improve the information ?