Technical FAQs

Ask a Question

What is the part number for the external reset mechanism for size 3 combination starter?

Issue:
What is the part number for the external reset mechanism for size 3 combo starter?

Product Line:
Non-Reversing Fusible Disconnect Switch Type

Environment:
Type S Combination Starters

Resolution:
To replace the reset mechanicanism you will need the following:
Qty 1 - 30019-113-59 - Reset sub-assembly (does not include the ring nut or gasket listed below).
Qty 1 - 30019-121-01 - Ring nut.
Qty 1 - 29206-30700  - Gasket (required on NEMA Type 12 enclosures).
Was this helpful?
What can we do to improve the information ?