Technical FAQs

Ask a Question

Are alternate lugs available for an EZM1600FS Series M02 Main fusible switch?

Issue:
Product Design Features

Product Line:
EZM Metering Equipment

Environment:
Alternate Main Lugs

Cause:
Application

Resolution:
Yes, this device uses a MJP22000Z60 Molded Case Switch as the Main with Class T fuses.
The standard mechanic lugs that come on the molded case switch from the factory, will accommodate (3) 3/0 - 500kcmil Max. Al/Cu wires per phase and neutral.

Mechanical Lugs:
1) For (2) 600kcmil Al/Cu Max. per phase and neutral use lug kit AL800P6K for the Molded Case Switch(requires one lug kit) and lug kit MMLK250 for the main neutral(requires one lug kit).
2) For (2) 750kcmil Max. Compact AL. ONLY per phase and neutral use lug kit AL800P7K for the Molded Case Switch(requires one lug kit) and a lug landing kit MMSK2 with the ILSCO lug TA8002N(Purchased separate).
3) For (4) 350kcmil Al/Cu Max. per phase and neutral use lug kit AL1200P24K for the Molded Case Switch(requires 2 lugs) and the standard neutral Lugs that come on the device.

NOTE: THE MAIN NEUTRAL OF THIS DEVICE WILL NOT ACCEPT COMPRESSION LUGS, SO NO ALTERNATE COMPRESSION LUGS ARE AVAILABLE.
Was this helpful?
What can we do to improve the information ?