Technical FAQs

Ask a Question

Do we offer a shaft extension for MD motor Disconnect switches?

Issue:
Customer looking for shaft extension for an MD motor disconnect switch

Product Line: 
Motor Disconnect Switches

Environment:
North American Products

Cause:
Need to panel door mounted device to control the motor disconnect switch MD

Resolution:
No shaft extension is available for this device, nor should it be necesarry as the device is enclosed. 
VLS switches and Vario switches may be a better fit for their application. 
 
Was this helpful?
What can we do to improve the information ?