Technical FAQs

Ask a Question

In the Process drive, where can the analog input signal be monitored?

Issue:
In the Process drive, where can the analog input signal be monitored?

Product Line:
Process ATV600 ATV900

Environment:
All models

Cause:
Need to see the analog input that the VFD recognizes

Resolution:
Analog input signals can be viewed in the VFD.

Navigate to the following and select:
Main menu
Display
I/O Map
Analog inputs image
Was this helpful?
What can we do to improve the information ?