Technical FAQs

Ask a Question

Is Part#: 9001BG202 Start-Stop push buttons (for latching Applications) maintained?

Issue:
Are the Push Buttons in a 9001BG202 control station momentary or maintained contact?
 
Product Line:
Push Buttons and Operator Interface

Environment:
North American Products

Cause:
Confirming 9001BG202 says for latching applications. The control station buttons has to be maintained

Resolution:
The pushbuttons are both maintained.
Was this helpful?
What can we do to improve the information ?