Technical FAQs

Ask a Question

What is the replacement cross rod for the XCKVR and XCKMR limit switches

Issue:      
Needs the part number for the two rods on the XCKVR / XCKMR limiit switch

Product Line:
Limit Switches

Environment:
Products sold and used in the United States

Cause:
Rod broke and would like to replace to use the limit switch

Resolution:
Rod 6 mm diagonal length, length 200 mm (7.87 in.) XCRZ03
Rod 6 mm diagonal length, length 200 mm (7.87 in.) with red mark XCRZ03R
 
Was this helpful?
What can we do to improve the information ?