Technical FAQs

Ask a Question

Induction Coil 31063-064-50 Voltage

Issue:
What is the output voltage of the induction coil 31063-064-50?

Product Line:
NEMA accessories - GIC Product

Environment:
US Product

Cause:
Product specifications

Resolution:
The coil outputs a 6V Voltage for illuminating a pilot light.
 
Was this helpful?
What can we do to improve the information ?