Technical FAQs

Ask a Question

Replacement Door Closing Handle for NEMA 12/3R Combination Starters size 1 or Smaller

Issue:
What is the part number for the replacement door closing handle (not disconnect handle) for a NEMA 12/3R Combination Starter size 1 or smaller?

Product Line:
NEMA Combination Starter - GIC Product

Environment:
US Product

Cause:
Component Replacement

Resolution:
The handle is available as part of the 9423M4 door closing mechanism kit and should be ordered as such.
Was this helpful?
What can we do to improve the information ?