Technical FAQs

Ask a Question

RPM2xxx Coil Information

Issue:
What is the consumption of the coil on an RPM2xxx relay?

Product Line:
General Purpose IEC Relays - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
DC coil units have an average consumption of 0.9 W
AC coil units have an average consumption of 1.2 VA
Was this helpful?
What can we do to improve the information ?