Technical FAQs

Ask a Question

What is the available through the door disconnect kit part number for Integral 18 starters?

Issue:
What is the available through the door disconnect kit for Integral 18?

Product Line:
Integral Starter

Environment:
North American Products

Resolution:
LA9LB331 is an integral door mounted handle assemble with an adjustable depth of 0 to 185 mm and black handle 

*Note: Integral starters are obsolete, for new applications a TeSys U line, or GV + TeSys D line combination should be selected. 
Was this helpful?
What can we do to improve the information ?