Technical FAQs

Ask a Question

Can the contacts in an XENG block be field converted?


Issue:
can we swap or replace the contact block assembly of  XENG3791

Product Line:
Push buttons and operator interface

Environment:
North American Products

Cause:
​Wants to swap the 1NC contact block of XENG3791 into a 1NO contact block

Resolution:
No, the entire XENG block will need to be removed and replaced. 
 
Was this helpful?
What can we do to improve the information ?