Technical FAQs

Ask a Question

What are the differences between Tesys F and Tesys D contactors?

Issue:
What are the differences between Tesys F and Tesys D contactors?

Product Line:
Contactors and Overload Relays

Environment:
TeSys™ D Contactors and Overload Relays
TeSys™ F Contactors and Overload Relays

Resolution:
- Tesys D amp range goes from 9A to 150A
- Tesys F amp range goes from 115A to 2100A
- Tesys F is dimensionally bigger
- Tesys D must be purchased with coil to be a complete part
- Tesys F contactors can be purchased without the coil, and the coil can be ordered seperately
- Lugs can be added to the Tesys F line in the field
Was this helpful?
What can we do to improve the information ?