Technical FAQs

Ask a Question

SoMove Crashes when attempting to Create a Project Offline.

Issue:
SoMove generated an error when attempting to create an offline project.  

Product Line:
SoMove 

Environment:
V2.6.2

Cause:
Corrupt XML file(s)

Resolution:
  • Close all running instances of SoMove
  • Delete all the .XML files from: C:\ProgramData\Schneider Electric\SoMove​ 
  • Re-start SoMove and check if running ok
If you are unable to find the C:\ProgramData\Schneider Electric\SoMove​ you will need to change your settings to show hidden files and folders.  
See attached document for details.
 
Was this helpful?
What can we do to improve the information ?