Technical FAQs

Ask a Question

Mounting track for 8501X Relay s

Issue:
Looking for Mounting bracket for 8 8501XDO60

Product Line: 
Operating Mechanism and Disconnect Switches

Environment:
North American Products

Cause:
There Customer is looking for a mounting bracket the will fit 8 8501X realy

Resolution:
To mount the 8501 type X relays we have the following track: 
9" long for 4 Relays - 8501XM4
18" long for 8 Relays - 8501XM8
27" long for 12 Relays - 8501XM12
36" long for 16 Relays - 8501XM16
72" long for 32 Relays - 8501XM32

Note: These relays do not mount to standard din rail. 
Was this helpful?
What can we do to improve the information ?