Technical FAQs

Ask a Question

Does the ATV320 drive have a 110V option card available?

Issue:
Does ATV320 Drive have a 110V option card available?

Product Line:
ATV320, Altivar 320

Environment:
All

Cause:
NA

Resolution:
ATV320 does not have a 110V input card available. Customer can use a 110V interposing relay instead and wire to Logic inputs.
Was this helpful?
What can we do to improve the information ?