Technical FAQs

Ask a Question

Alternate lugs for FA and FH breakers

Product Line:
Circuit Breakers

Resolution:

Alternate Lugs for FA and FH Breaker

Al Lugs for use with Al or Cu wire:


FA/FH Breaker - 15-30A / 35-100A 
(1) 14–4 AWG Cu or (1) 12–4 AWG Al 
AL50FA

FA/FH Breaker - 35-100A / 15-30A 
(1) 14–1/0 AWG Cu or (1) 12–1/0 AWG Al
AL100FA 

FA/FH Breaker - 15-100A 
(1) 12–3 AWG Cu 
AL100TF 
(For use in the OFF end only, when the OFF end is the load end)


Cu Lugs for use with Cu Wire Only:

FA/FH Breaker - 15–100 A
(1) 14–1 AWG Cu 
CU100FA

FA/FH Breaker - 15-100A 
(1) 12–3 AWG Cu
CU100TF
(For use in the OFF end only, when the OFF end is the load end)
 
Was this helpful?
What can we do to improve the information ?