Technical FAQs

Ask a Question

TeSys N Auxiliary Contacts

Issue:
What auxiliary contacts are used with the TeSys N contactors and starters?

Product Line:
TeSys N - GIC Product

Environment:
US Product

Cause:
Product Specification

Resolution:
The LADNxx  auxiliary contact blocks which are used with the TeSys D and the TeSys F contactors are also used with the TeSys N.
See attached table for selection. 

Note: 
  1. For spring terminal versions of these blocks, add a 3 to the end of the catalog number (for example, LADN223). For slip-on versions, add 9 to the end of the catalog number (for example, LADN229).
  2. Including 1 N.O. + 1 N.C. make-before-break overlapping contacts.
Was this helpful?
What can we do to improve the information ?