Technical FAQs

Ask a Question

Through-the-door Accessories for VLS8M2

Issue:
Is there a handle and shaft that can be used with VLS8M2 to provide through-the-door operation?

Product Line:
IEC Disconnect- GIC Product

Environment:
US Product

Cause:
Product Specification

Resolution:
Yes, can only be used with 7mm shaft and pistol handle VLSH3S7BD/VLSH3S7RD
Was this helpful?
What can we do to improve the information ?