Technical FAQs

Ask a Question

Changing the Overload on a NEMA Starter

Issue:
Will changing the overload on a NEMA starter void the UL label?

Product Line:
NEMA Starters - GIC Product

Environment:
US Product

Resolution:
Changing the overload is not a UL component recognized kit modification.  As such, changing the overload will nullify the part number on the label and void the UL label.  This modification should be made by a UL panel shop.
Was this helpful?
What can we do to improve the information ?