Technical FAQs

Ask a Question

What are these fault codes on my System Control Panel? (Ex. F808, F774)

Issue
The System Control Panel issued three digit fault codes that are not listed in any documentation.

Product Line
System Control Panel

Environment
SCP updated to firmware v2.02, and use with MPPT controllers, or Conext inverters

Resolution
At the time of this writing, a new firmware containing the fix has not yet been released.  The correct fault codes can found via the Fault Logs for the specific units.  These will be in the following tree:

System Devices -> <Enter unit name here> -> View Device Info -> View Fault Log

Cause
This was caused by a bug in the in the compiler use to built the SCP v2.02 firmware.
Was this helpful?
What can we do to improve the information ?