Technical FAQs

Ask a Question

What is the difference between the NF102OE and NQ102OE labels?

Issue:
What is the difference between the  NF102OE and NQ102OE labels?

Product Line:
Panel accessories

Environment:
NQ panel accessories and NF panel accessories

Cause:
Product features

Resolution:
The NQ102OE labels are 3/4`` H and 1/2`` wide. 
The NF102OE is 1" H x 1/2" wide.
The difference is the NF uses larger size of breakers than NQ so the NQ102OE labels cannot be used on a NF panel nor visa versa
Was this helpful?
What can we do to improve the information ?