Technical FAQs

Ask a Question

There are two arrows on the GV3P dial - which one should we use?

Issue:  
How is the dial on the front of the GV3P manual starter set? 

Product Line:
IEC Contactors and Starters

Environment:
GV3P Manual Starters and Protectors

Cause:
Installation
 
Resolution:
Per the attached instruction bulletin the black arrow should be used when the GV3P is utilized as a stand alone device, when the GV3P is mounted to an LC.D contactor the arrow dial should be used. 

Was this helpful?
What can we do to improve the information ?