Technical FAQs

Ask a Question

What is the part number for the fuse clips only for the 9422TDF60 disconnect switch?

Issue:
What is the part number for the fuse clips only for the 9422TDF60 disconnect switch? 

Product Line:
9422 Disconnect Switches - GIC Product

Environment:
US Product

Cause:
Customer needs replacement fuse clips only. 

Resolution:
The fuse clips only (3 clips and screws per bag) for the 9422TDF60 disconnect switch is part number 31301-512-51. 
Was this helpful?
What can we do to improve the information ?