Technical FAQs

Ask a Question

What type of material is the handle in a 9421LN1 kit made of?

Issue:
What type of material is the 9421LN1 handle made of?

Product Line:
Operating Mechanisms for Circuit Breakers

Environment:
North American Products

Resolution:
The 9421LH6 handle this utilizes is made of Die Cast Zinc, as is the base ring itself. 
The shafts in this kit are steel bar stock, and the mechanisms are all steel construction.
Was this helpful?
What can we do to improve the information ?