Technical FAQs

Ask a Question

What is the maximum breaker that can be installed in the QONQ42MS400?

Issue:
Need to know the maximum amperage of breaker that can be installed.

Product Line:
QO Panels

Environment:
QO Panels

Cause:
Breaker sizing

Resolution: 
QO2200VH is the maximum breaker size.
 
Was this helpful?
What can we do to improve the information ?