Technical FAQs

Ask a Question

What is the part number for an end cap for RWT06S60S or a RWT06S60?

 Issue:
What is the part number for the end caps for the RWT wallduct?

Product Line:
wallduct

Environment:
Class 5250 - wallduct type RWT

Cause:
Product selection

Resolution:
The part numbers for the RWT end caps are as follows:
RWT06EC - 6"
RWT10EC - 10"
RWT18EC - 18"
These can be found in the online Digest by using the link below:
http://www.schneider-electric.us/en/work/support/resources-and-tools/digestplus/
Was this helpful?
What can we do to improve the information ?