Technical FAQs

Ask a Question

Did Square D offer a Non-Linear NEHB Panelboard?

Issue:
Were NEHB panels offered as Non Linear Load panels?

Product Line:
Panelboards

Environment:
NEHB panelboard

Cause:
Product features.

Resolution:
Yes, Square D did make a Non-Linear NEHB Panelboard before but NEHB panelboards are now obsolete. 
The suffix NL in the interior part number (ex. NEHB42441-2NL) signifies that the interior is rated for Non-Linear Loads (200% rated neutral).


 
Was this helpful?
What can we do to improve the information ?