Technical FAQs

Ask a Question

Is a Size 00 Nema starter available in a Nema 3R or Nema 12 enclosure?

Issue:
Is a Size 00 Nema FVNR starter available in a Nema 3R/12 enclosure:

Product Line:
Nema FVNR starters sold and supported in the USA.

Issue:
Application

Cause:
Environment

Resolution:
No, a Size 0 starter must be selected for Nema 3R/12 enclosure. 

 
Was this helpful?
What can we do to improve the information ?