Technical FAQs

Ask a Question

LOOKING FOR A LOAD CENTER COVER TO FIT AN OLDER SQD PANEL. CAT# IS 26-614H

Issue:
Needs a cover for a load center.

Product Line:
Load Centers

Environment:
Residential

Cause:
Missing cover

Resolution: 
The QO26-614H and HA style can be found in the 1970 Digest.  No spare mechanical parts are available for this load center.  The box dimensions are 12 1/8" wide by 26 1/8" tall.
QO Breakers can be used in this panel.
Was this helpful?
What can we do to improve the information ?