Technical FAQs

Ask a Question

How many partitions can be added to the RWT wall duct and how wide can they be?

Issue:
What is the maximum width of the compartments that can be made using partitions for the RWT wall duct?

Product Line:
Wall duct

Environment:
RWT

Resolution:
Our recommendation when using partitions is for a 3 inch wide compartment.  Based on our recommendations, (1) partition would be suitable for the 6 inch wall duct; (2) partitions for the 10 inch duct and (5) partitions for the 18 inch wall duct. The formed dimension of the bottom leg of the partition, it is 0.81" from outside of form to edge of steel.
Was this helpful?
What can we do to improve the information ?