Technical FAQs

Ask a Question

How Many Plug in Openings are Available in Enhanced Powerbus Busway?

Issue:
How many plug in openings are available in enhanced Powerbus?

Product Line:
225A to 400A Powerbus sold and supported in the USA.

Environment:
Product features

Cause:
Installation

Resolution:
Standard Powerbus has ten plug in openingins per ten foot length (five per each side).  Enhanced Powerbus has twenty openings per ten foot section (ten per each side.)
Enhanced Powerbus is available in 225A through 400A.  
PBCP****  is standard Powerbus
PBCE*** is enhanced Powerbus. 
Was this helpful?
What can we do to improve the information ?