Technical FAQs

Ask a Question

What is suffix 5238?

Issue:
When a breaker catalog number has suffix 5238, what does that mean?

Product Line:
Circuit Breakers

Environment:
Breakers that have suffix "5238"

Resolution:
Suffix 5238 signifies (for QO) low amp connector with high amp material, without clamp plate and with 10-32 screw for these breakers
  • 1P 35A‐60A
  • 2P 35A‐60A
  • 3P 35A‐50A
If GFI/EPD, low amp connector, without clamp plate and with 10-32 screw, 35A‐60A, UL approved.
Was this helpful?
What can we do to improve the information ?