Technical FAQs

Ask a Question

CANOpen scaling for LXM28

Issue:
CANOpen scaling for LXM28

Product Line:
LXM28

Resolution:

On CANopen, the scaling factor will be adjusted using parameters 6092:01 (Feed; [USER units]) and 6092:02 (Shaft Revolutions).
Parameters 6091:01 (Motor revolutions) and 6091:02 (Shaft revolutions) can be used to adjust an additional GearRatio.

Was this helpful?
What can we do to improve the information ?