Technical FAQs

Ask a Question

RUMC and RUMF Response Time

Issue:
What is the coil pickup and dropout response time for the RUMC and RUMF relays?

Product Line:
IEC Relays - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
These units have a 20ms max pick up (100% coil voltage) and 20ms max drop-out.
Was this helpful?
What can we do to improve the information ?