Technical FAQs

Ask a Question

9007CLS1 with Other Contact Arrangements

Issue:
Is the 9007CLS1 offered with 1NO and 1NC contacts or any other contact arrangement than the 1 NC slow break?

Product Line:
9007 Heavy Duty Limit Switches - GIC Product

Environment:
US Product

Cause:
Product Selection

Resolution:
The 9007CLS1 is only made with the one NC slow break contact.  This type of application requires a positive opening contact, and the only positive opening NC contact in the 9007C lineup is the slow break NC contact utilized in this switch.
Was this helpful?
What can we do to improve the information ?