Technical FAQs

Ask a Question

LC1D40 or LC1D80 with "M" Suffix

Issue:
What does the "M" suffix mean for a LC1D contactor?

eg LC1D40M or LC1D80M printed on front cover, full part numbers LC1D40G7M, LC1D40U7M, LC1D80G7M, LC1D80U7M

Product Line:
LC1D Contactors - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
"M" Suffix is designation for removal of front plate.  Use the full part number without the "M" for replacement.
Was this helpful?
What can we do to improve the information ?